MCF5235 - Occasional startup failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5235 - Occasional startup failure

5,471件の閲覧回数
nxf51434
NXP Employee
NXP Employee

Hi guys, my customer met the low probability issue of startup failure with the BPKT level is pulled down during the rising process. That's the confusion that BKPT (BDM mode) is input and pulled up to vdd with a 4.7k resistor. Who controls the BKPT pin?

BKPT FAILED.png

Additionally, I checked the customer schematic and found that the XTAL was floating, against to the description on the 782 page of the manual says that XTAL must be tied low in extern clock mode when reset is asserted, or clocks 'may be suspended indefinitely'. I'm not sure if this is the root cause.

sch2.png

0 件の賞賛
返信
8 返答(返信)

5,311件の閲覧回数
TomE
Specialist II

We have multiple devices using the MCF5235. They're all the same basic design. They all have XTAL floating and are using an external oscillator, and we've never had any problems. Everything says BKPT is an input, so I don't know why it is going low like that. Are you sure there are no shorts to other signals on the board?

You have a 3ms rise time on VDD there. What's the timing of the RESET pin relative to those signals? Our design uses a separate POR chip that holds RESET low for a while after VDD has come up (and the oscillator has stabilised). Is your one doing that, or is it relying on the internal POR circuitry? What's the assertion of RSTOUT relative to those signals you're looking at. Both when it works and when it doesn't?

What's JTAGEN connected to? We have a 2k2 Pullup on that. If that is floating then the chip might get confused between JTAG and Debug modes.

Tom

 

5,377件の閲覧回数
nxf51434
NXP Employee
NXP Employee

Your information is helpful, appreciated!

0 件の賞賛
返信

5,417件の閲覧回数
_angelo_
Contributor III

hi nxf51434

from your diagram, it is not visible what's connected to BKPT. It is an input, active low, so i would eventually put a 4,7K pull up there, for testing.

Is it possible in your custom board some dirty or short brings the signal down ? 

Cheers 

0 件の賞賛
返信

5,374件の閲覧回数
nxf51434
NXP Employee
NXP Employee

I suggested customer pulled up JTAG_EN to reduce the risk of BKPT triggered by dirty signals. TKS!

0 件の賞賛
返信

5,465件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I checked customer board schematics with CLKMOD[1:0] equals 10 setting is used (normal PLL mode with external clock reference), which was mentioned at MCF5235 chip errata file with below description:

Hui_Ma_0-1648609347358.png

Please try with this workaround and check if it could fix the issue.

Wish it helps.

Mike

0 件の賞賛
返信

5,459件の閲覧回数
nxf51434
NXP Employee
NXP Employee

Hi Hui, I checked errata SECF131 and SECF163 before, customer design has already connected CLKMOD1 to RSTI, and the chip date date is xxxx1748, newer than the xxxx1031. 

0 件の賞賛
返信

5,440件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Stevens,

The BKPT pin is the input pin, which used to puts the core into a halted state after the current instruction completes.

I did a search with internal support records and could not find any info about this phenomenon. 

When customer connect the XTAL pin to GND, if that could reduce the failure happen frequence?

During the POR phase, if customer assert the MCF5235 reset button, if that could help to reduce the failure happen frequence? I want to check if external clock source could provide stable reference clock during PLL initialization phase.

If that issue is a single board issue? 

best regards,

Mike

0 件の賞賛
返信

5,375件の閲覧回数
nxf51434
NXP Employee
NXP Employee

The issue is not single board case and difficult to reproduce. XTAL pin was't drawn out due to BGA packaging. I'd advised customer to layout new board to reduce the risk. TKS!

0 件の賞賛
返信