MCF5235 FlexCAN transmits continuously

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCF5235 FlexCAN transmits continuously

跳至解决方案
1,698 次查看
JulienP
Contributor II

Hello,


I'm running into a very strange problem with the FlexCAN. Quick example:

- I'm trying to transmit 0x18DAEEFB | 02-10-7E-FF-FF-FF-FF-BB. It is sent once, no errstat or errcnt, it works fine.

- I'm trying to transmit 0x18DAEEFB | 02-10-7E-FF-FF-FF-FF-CC. FlexCAN is transmitting continuously, errcnt is inscreasing, BIT1ERR, BUSOFF and others bit error are set (BUSOFF interrupt is disabled). The Control/Status register of the MB remains activate. The only way to stop this mess is to set the MB to inactive state by myself. Of course, the frame is sent to the same target, and there are no differences between those two frames for the target. In addition, the target is answering many times as well.

- All the frames are transmitted well (once) using LoopBack mode.

 

This is just one example, but it is doing the same with many frames. My functions are in attachment.

 

Do I do something wrong?

标签 (1)
0 项奖励
回复
1 解答
1,021 次查看
JulienP
Contributor II

I solved it using EXTAL clock instead of PLL clock!

 

Bye!

 

Julien.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,021 次查看
Britti1982
Contributor I

I'm new in the world MQX
 I work with MCF5225evb recently and I am trying the sample project for use on the FlexCAN demoboard.
 making debugging and looking CANL and CANH bus oscilloscope I see that the frames are continuous, even if I start with debugging in the STOP condition.
 Why does this happen?
 and then because the serial transmission is complete even if there are other nodes send their ACKs connected on the bus?

help me please.

0 项奖励
回复
1,022 次查看
JulienP
Contributor II

I solved it using EXTAL clock instead of PLL clock!

 

Bye!

 

Julien.

0 项奖励
回复