MCF522XX Part identification number inside CIR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF522XX Part identification number inside CIR

3,993件の閲覧回数
MrBean
Contributor I

Chip Identification Register (CIR) ( IPSBAR+0x11000A )
Part identification number (PIN) (bits 15:6 of CIR)

I'd like to know the PINs of the following parts:

 

MCF52210

MCF52211

MCF52212

MCF52213

 

MCF52236

 

Thanx

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,036件の閲覧回数
TomE
Specialist II

The table got corrupted (all jammed into one line) in one of the forum software conversions. Here it is again:

 

#define COLDFIRE_ID  (0x48 << 6)  // ID for 52230
#define COLDFIRE_ID  (0x49 << 6)  // ID for 52231
#define COLDFIRE_ID  (0x4a << 6)  // ID for 52233
#define COLDFIRE_ID  (0x4b << 6)  // ID for 52234
#define COLDFIRE_ID  (0x4c << 6)  // ID for 52235
#define COLDFIRE_ID  (0x4d << 6)  // ID for 52232
#define COLDFIRE_ID  (0x4e << 6)  // ID for 52236
#define COLDFIRE_ID  (0x50 << 6)  // ID for 52221
#define COLDFIRE_ID  (0x53 << 6)  // ID for 52223
#define COLDFIRE_ID  (0x83 << 6)  // ID for 52252 (512k FLASH / 64k SRAM 100 LQFP)
#define COLDFIRE_ID  (0x84 << 6)  // ID for 52252 (512k FLASH / 32k SRAM 100 LQFP)
#define COLDFIRE_ID  (0x85 << 6)  // ID for 52254 (256k FLASH / 64k SRAM 100 LQFP)
#define COLDFIRE_ID  (0x86 << 6)  // ID for 52254 (256k FLASH / 32k SRAM 100 LQFP)
#define COLDFIRE_ID  (0x87 << 6)  // ID for 52252C (512k FLASH / 64k SRAM 100 LQFP)
#define COLDFIRE_ID  (0x88 << 6)  // ID for 52252C (512k FLASH / 32k SRAM 100 LQFP)
#define COLDFIRE_ID  (0x89 << 6)  // ID for 52254C (256k FLASH / 64k SRAM 100 LQFP)
#define COLDFIRE_ID  (0x8a << 6)  // ID for 52254C (256k FLASH / 32k SRAM 100 LQFP)
#define COLDFIRE_ID  (0x8b << 6)  // ID for 52256 (512k FLASH / 64k SRAM 144 LQFP or MAPBGA)
#define COLDFIRE_ID  (0x8c << 6)  // ID for 52256 (512k FLASH / 32k SRAM 144 LQFP or MAPBGA)
#define COLDFIRE_ID  (0x8d << 6)  // ID for 52258 (256k FLASH / 64k SRAM 144 LQFP or MAPBGA)
#define COLDFIRE_ID  (0x8e << 6)  // ID for 52258 (256k FLASH / 32k SRAM 144 LQFP or MAPBGA)
#define COLDFIRE_ID  (0x8f << 6)  // ID for 52256C (512k FLASH / 64k SRAM 144 LQFP or MAPBGA)
#define COLDFIRE_ID  (0x90 << 6)  // ID for 52258C (256k FLASH / 64k SRAM 144 LQFP or MAPBGA)
#define COLDFIRE_ID  (0x91 << 6)  // ID for 52255C (512k FLASH / 64k SRAM 100 LQFP)
#define COLDFIRE_ID  (0x92 << 6)  // ID for 52259C (512k FLASH / 64k SRAM 144 LQFP or MAPBGA)
0 件の賞賛
返信

3,177件の閲覧回数
mjbcswitzerland
Specialist V

Hi Mr Bean

 

Here's my list - which I have collected over the years... Can't guaranty 100% but the best I have at the moment:

 

#define COLDFIRE_ID       (0x48 << 6)                                  // ID for 52230#define COLDFIRE_ID       (0x49 << 6)                                  // ID for 52231#define COLDFIRE_ID       (0x4a << 6)                                  // ID for 52233#define COLDFIRE_ID       (0x4b << 6)                                  // ID for 52234#define COLDFIRE_ID       (0x4c << 6)                                  // ID for 52235#define COLDFIRE_ID       (0x4d << 6)                                  // ID for 52232#define COLDFIRE_ID       (0x4e << 6)                                  // ID for 52236#define COLDFIRE_ID       (0x50 << 6)                                  // ID for 52221#define COLDFIRE_ID       (0x53 << 6)                                  // ID for 52223#define COLDFIRE_ID       (0x83 << 6)                                  // ID for 52252 (512k FLASH / 64k SRAM 100 LQFP)#define COLDFIRE_ID       (0x84 << 6)                                  // ID for 52252 (512k FLASH / 32k SRAM 100 LQFP)#define COLDFIRE_ID       (0x85 << 6)                                  // ID for 52254 (256k FLASH / 64k SRAM 100 LQFP)#define COLDFIRE_ID       (0x86 << 6)                                  // ID for 52254 (256k FLASH / 32k SRAM 100 LQFP)#define COLDFIRE_ID       (0x87 << 6)                                  // ID for 52252C (512k FLASH / 64k SRAM 100 LQFP)#define COLDFIRE_ID       (0x88 << 6)                                  // ID for 52252C (512k FLASH / 32k SRAM 100 LQFP)#define COLDFIRE_ID       (0x89 << 6)                                  // ID for 52254C (256k FLASH / 64k SRAM 100 LQFP)#define COLDFIRE_ID       (0x8a << 6)                                  // ID for 52254C (256k FLASH / 32k SRAM 100 LQFP)#define COLDFIRE_ID       (0x8b << 6)                                  // ID for 52256 (512k FLASH / 64k SRAM 144 LQFP or MAPBGA)#define COLDFIRE_ID       (0x8c << 6)                                  // ID for 52256 (512k FLASH / 32k SRAM 144 LQFP or MAPBGA)#define COLDFIRE_ID       (0x8d << 6)                                  // ID for 52258 (256k FLASH / 64k SRAM 144 LQFP or MAPBGA)#define COLDFIRE_ID       (0x8e << 6)                                  // ID for 52258 (256k FLASH / 32k SRAM 144 LQFP or MAPBGA)#define COLDFIRE_ID       (0x8f << 6)                                  // ID for 52256C (512k FLASH / 64k SRAM 144 LQFP or MAPBGA)#define COLDFIRE_ID       (0x90 << 6)                                  // ID for 52258C (256k FLASH / 64k SRAM 144 LQFP or MAPBGA)#define COLDFIRE_ID       (0x91 << 6)                                  // ID for 52255C (512k FLASH / 64k SRAM 100 LQFP)#define COLDFIRE_ID       (0x92 << 6)                                  // ID for 52259C (512k FLASH / 64k SRAM 144 LQFP or MAPBGA)

 

Regards

 

Mark

 

www.uTasker.com

 

 

0 件の賞賛
返信

3,177件の閲覧回数
MrBean
Contributor I

Mark, thanx for the 52232 and 52236, didnt have those.

 

Does anyone know the pin's for the MCF5221x series ?

0 件の賞賛
返信