MCF52277RM - 4 wire resistive touch panel interface.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52277RM - 4 wire resistive touch panel interface.

1,061件の閲覧回数
anujtopiwala
Contributor I

Using MCF52277RM I need to establish 4 wire resistive touch panel interface. But I have 6-8 inch cable extending from the touch panel to main board. Will the inbuilt Touch controller with ADC biasing circuit be enough for noise free interface. The touch panel resistance is 200 ~900 ohm both x and y side with < 1.5 % linearity.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)