MCF52264AF80 - where are the details?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF52264AF80 - where are the details?

757 次查看
mjbcswitzerland
Specialist V

Hi All

I just noticed that there is an active device called the MCF52264AF80 and it also shows up at many distributors but all information points to the M52259 data sheet/user's manual where this is not mentioned.

It looks to be much like an M52252 but with 80MHz top speed and 0..105° temperature range in 100 pin LQFP.

Does any one know more?

Regards

Mark

标签 (1)
0 项奖励
回复
1 回复

655 次查看
yibbidy
Contributor V

A parametric search on the Freescale website shows that it is very similar to the 52259 except that it has 256kB flash and 32kB ram.  Obviously there must be more differences, it is very odd that there is no datasheet.

 

Shaun

 

0 项奖励
回复