MCF52259 - Reading ADC-Modul with DMA-Request (DMA-Timer)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF52259 - Reading ADC-Modul with DMA-Request (DMA-Timer)

2,118 次查看
sven_kaemmer
Contributor III

Hello,

 

i want to read the ADRSLTn-Registers with a DMA-Request. I used an DMA-Timer which request periodically a DMA-Transfer. The problem is that the RDY-Bits in the ADSTAT no be cleared. So i get always the same result. The ADC runs in loop-Mode with fastest speed, so an complete measurement is much faster then the DMA-Timer. Can everyone help me? Thanks.

标签 (1)
0 项奖励
回复
3 回复数

1,054 次查看
scifi
Senior Contributor I

I implemented ADC data collection with DMA. The purpose was to reduce noise by averaging. I set up a buffer to collect 128 samples of each channel, a DMA channel and a DMA timer. The DMA timer was configured to trigger at the rate of the ADC or slower. Works great. I didn't encounter any issues with the RDY bits. One funny thing I noticed: for some reason the ADRSLTn registers' addresses are not aligned to a 16-byte boundary, they are off by 2 bytes. This isn't good for DMA since it likes aligned addresses, so some buffer memory is wasted.

0 项奖励
回复

1,054 次查看
sven_kaemmer
Contributor III

Hi Scifi, I think I do it the same way, only the buffer is smaller. I get only a correct value from the ADC when I read the ADC normally between the DMA-Transfers. My intention was also to reduce noise by averaging. Can you post me some parts of your code or correct my code? Many thanks before...

 

  MCF_DMA_DMAREQC =   MCF_DMA_DMAREQC_DMAC0(4); 
 
MCF_DMA0_SAR = MCF_DMA_SAR_SAR(0x40190012);
  
MCF_DMA0_DAR = MCF_DMA_DAR_DAR((uint_32)&dma_adc_array[0]);

  
MCF_DMA0_BCR = MCF_DMA_BCR_BCR(16);
  
MCF_DMA0_DCR = MCF_DMA_DCR_START      |
                 
MCF_DMA_DCR_DSIZE_BYTE |
                 
MCF_DMA_DCR_DINC       |
                 
MCF_DMA_DCR_SSIZE_BYTE |
                 
MCF_DMA_DCR_SINC       |
                 
MCF_DMA_DCR_EEXT;

 

  MCF_DTIM0_DTXMR = MCF_DTIM_DTXMR_DMAEN;
  
MCF_DTIM0_DTER = MCF_DTIM_DTER_REF;
  
MCF_DTIM0_DTRR = 200;
  
MCF_DTIM0_DTMR = MCF_DTIM_DTMR_RST      |
                   
MCF_DTIM_DTMR_CLK_DIV1 |
                   
MCF_DTIM_DTMR_FRR      |
                   
MCF_DTIM_DTMR_ORRI     |
                   
MCF_DTIM_DTMR_PS(15);

0 项奖励
回复

1,054 次查看
scifi
Senior Contributor I

The comments in my code are not in English, so I stripped them before posting:

 

 

#include "adc.h"#include "config.h"#include "mcf52233regs.h"#include "irq.h"#define ADC_CTRL1       MCF_REG16(0x190000)#define ADC_CTRL2       MCF_REG16(0x190002)#define ADC_POWER       MCF_REG16(0x190052)#define ADC_ADZCSTAT    MCF_REG16(0x190010)#define ADC_RSLT7       MCF_REG16(0x190020)#define CTRL_START      (1 << 13)#define CTRL_STOP       (1 << 14)#define CTRL_SIMULT     (1 << 5)#define POWER_PD0       (1 << 0)#define POWER_PD1       (1 << 1)#define POWER_PD2       (1 << 2)#define POWER_PSTS0     (1 << 10)#define POWER_PSTS1     (1 << 11)#define DMA_DMAREQC     MCF_REG32(0x14)#define DMA_SAR0        MCF_REG32(0x100)#define DMA_DAR0        MCF_REG32(0x104)#define DMA_BCR0        MCF_REG32(0x108)#define DMA_DCR0        MCF_REG32(0x10C)#define DMAREQC_DTIM0   4#define DCR_INT         (1u << 31)#define DCR_EEXT        (1 << 30)#define DCR_CS          (1 << 29)#define DCR_AA          (1 << 28)#define DCR_SINC        (1 << 22)#define DCR_SSIZE_WORD  (2 << 20)#define DCR_DINC        (1 << 19)#define DCR_DSIZE_WORD  (2 << 17)#define DCR_SMOD_16     (1 << 12)#define DCR_DMOD_2K     (8 << 8)#define DCR_D_REQ       (1 << 7)#define DSR_DONE        (1 << 24)#define SCM_MPARK       MCF_REG32(0x1C)#define SCM_MPR         MCF_REG8(0x20)#define MPARK_BCM24BIT  (1 << 24)#define DTIM_PERIOD     40#define DMA_INT_NUM     9#define DMA_INT_VECT    292#define ADC_NCHANNELS   8#define ADC_PORT_MASK   0x3F#define ADC_NSAMPLES    128#define DMA_NBYTES      ((((1<<24) - 1) / sizeof(buffer)) * sizeof(buffer))#define ADC_MODE        3#define ADC_CLK_DIV     2#define DTIM_NUM        0#define DCR_DMOD        DCR_DMOD_2K#pragma ghs section sbss=".adcbuf"static uint16_t buffer[ADC_NSAMPLES][ADC_NCHANNELS];#pragma ghs sectionIRQ_HANDLER_PREFIXvoidadc_dma0_handler(void){        DMA_BCR0 = DSR_DONE;        DMA_BCR0 = DMA_NBYTES;        DMA_DCR0 = DCR_INT | DCR_EEXT | DCR_CS |                   DCR_SINC | DCR_SSIZE_WORD |                   DCR_DINC | DCR_DSIZE_WORD |                   DCR_SMOD_16 | DCR_DMOD_2K | DCR_D_REQ;}#pragma intvect adc_dma0_handler DMA_INT_VECTstatic voidconfig_dma(uint8_t level, uint8_t prio){        SCM_MPR |= (1 << 2);        SCM_MPARK |= MPARK_BCM24BIT;        DMA_DMAREQC = DMAREQC_DTIM0;        DMA_SAR0 = (uint32_t)&ADC_ADZCSTAT;        DMA_DAR0 = (uint32_t)buffer;        DMA_BCR0 = DMA_NBYTES;        DMA_DCR0  = DCR_INT | DCR_EEXT | DCR_CS |                    DCR_SINC | DCR_SSIZE_WORD |                    DCR_DINC | DCR_DSIZE_WORD |                    DCR_SMOD_16 | DCR_DMOD_2K | DCR_D_REQ;        irq_config(DMA_INT_NUM, level, prio, adc_dma0_handler);        irq_unmask(DMA_INT_NUM);        DTIM_DTXMR(DTIM_NUM) = DTXMR_DMAEN;        DTIM_DTRR(DTIM_NUM)  = DTIM_PERIOD;        DTIM_DTMR(DTIM_NUM)  = DTMR_ORRI | DTMR_FRR |                               DTMR_CLK_DIV1 | DTMR_RST;}voidadc_init(uint8_t level, uint8_t prio){        GPIO_PANPAR = ADC_PORT_MASK;        ADC_CTRL1 = CTRL_STOP | ADC_MODE;        ADC_CTRL2 = CTRL_STOP | CTRL_SIMULT | ADC_CLK_DIV;        ADC_POWER &= ~(POWER_PD0 | POWER_PD1 | POWER_PD2);        while ((ADC_POWER & (POWER_PSTS0 | POWER_PSTS1)) != 0)        {        }        ADC_CTRL1 &= ~CTRL_STOP;        ADC_CTRL1 |= CTRL_START;        config_dma(level, prio);}uint16_tadc_read(uint8_t channel){        if (channel == 7)        {                return ADC_RSLT7;        }        else        {                int32_t sum = 0;                uint8_t i;                for (i = 0; i < ADC_NSAMPLES; i++)                {                        sum += buffer[i][channel + 1];                }                sum /= ADC_NSAMPLES;                return (uint16_t)sum;        }}

 

 

0 项奖励
回复