MCF52259 Internal Flash Read/write Cycle Lifetime

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF52259 Internal Flash Read/write Cycle Lifetime

1,875 Views
easybreather
Contributor II

Hi

It would be great to settle an internal argument here
Does anyone know what the Internal Flash read/write lifetime is?
i.e. for standard Intel/AMD flash devices, you get 100000 read/writes for a device.
Is this same for MCF52259?

Cheers!

Labels (1)
0 Kudos
Reply
2 Replies

1,628 Views
TomE
Specialist II

It is clearly marked in the MCF52259 data sheet:

 

2.4 Flash Memory Characteristics
The flash memory characteristics are shown in Table 9 and Table 10.

Table 10. SGFM Flash Module Life Characteristics

 

Maximum number of guaranteed program/erase cycles1 before failure P/E 10,000 Cycles
Data retention at average operating temperature of 85°C Retention 10 Years

 

===

 

I vaguely remember an errata item for a Freescale product stating the cycle limit for "large blocks" was something like 100(!), but the small blocks could be rewritten a lot more times. Can anyone remember which part this was?

 

Tom

 

 

 

0 Kudos
Reply

1,628 Views
easybreather
Contributor II

Tom,

I must be blind - thanks for pointing out my inabilitiy to read!
10K cycles is not sparkling but better than the 1K cycles someone was trying to convince me of...

 

Thanks again!
eb

0 Kudos
Reply