MCF52254 Reset Hangs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF52254 Reset Hangs

1,544 次查看
salman83
Contributor II

Hi,

 

I am trying to do software reset but everytime during the reset it is unable to boot. It looks like that it is hanged. Even if I do the hardware reset, still it does not respond. I have to power down the mcu and then power it up again.

 

I tried to do the reset using two ways: -

 

- Asserting Software Reset Bit

- Backup Watchdog Timer Expiration

 

Both of them do not work at all.

 

Here is code for each section: -

 

Software Reset

----------------------

MCF_RCM_RCR = MCF_RCM_RCR_SOFTRST | MCF_RCM_RCR_FRCRSTOUT;

 

 

 

Backup Watchdog Timer

------------------------------------

MCF_CLOCK_BWCR = 0x00;
MCF_BWT_WMR = 0xFFFF;
MCF_BWT_WCR = MCF_BWT_WCR_EN;

 

while(1) { }

 

 

 

Thanks in advance for the help.

 

Regards.

标签 (1)
0 项奖励
回复
1 回复

1,367 次查看
TomE
Specialist II

Type "mcf52259 soft reset" into the Search Field and see if any of the previous posts on this topic give a solution.

Here's someone who now has soft reset working fine. There must be a difference between his hardware and yours:

Re: Software Reset For MCf52259

Here's one from 2011 stating that the M52259DEMO Board doesn't soft-reset, but the M52259EVB Board does work. Also that it doesn't work with the debugger connected.

Re: MCF52259: Software Reset hangs

That should be enough to get you working.

Tom

0 项奖励
回复