MCF52235 Family

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52235 Family

1,152件の閲覧回数
michaelkwan
Contributor I

MCF52235 datasheet note 3 on page 21 stated that "The use of an external PHY limits ADC, interrupt, and QSPI functionality. It also disables the UART0/1 and timer pins." I plan to use the external PHY on my design, I would like to make sure those pins/bits within those limited functions which are NOT mapped to the Ethernet internal signals(FEC_*) still available as user's I/Os?

Thanks!

Michael

ラベル(1)
1 返信

1,063件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Yes, you can disable the internal PHY and connect an external PHY. As the manual mentioned when using an external PHY, some pins that are multiplexed with the MII are no longer usable. datasheet shows the signals used for an external interface.