MCF52233DEMO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF52233DEMO

1,813 Views
sharda
Contributor II

Hi all,

Has anybody worked on .S19 uploading through ethernet using MCF52233DEMO board........

Plz give your email id to [email protected]

 

-Sharda

Labels (1)
0 Kudos
Reply
1 Reply

1,130 Views
RichTestardi
Senior Contributor II

Hi,

 

If you want to see S19 parsing and upload thru Ethernet, I have an example in my skeleton source code project, skeleton.zip, at the bottom of this page:

 

  http://www.cpustick.com/downloads.htm

 

Basically, that skeleton will build a command-line interface for about a dozen different MCUs -- you only need to follow the MCF52233 #if's.  Most of the code you care about is in flash_upgrade(), in sources/flash.c.  You can enter an "upgrade" command and then paste an S19 file into a terminal emulator window connected to port 1234 of the DHCP address, and the system will upgrade its flash memory.

 

-- Rich

0 Kudos
Reply