MCF52233 - Code protection ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52233 - Code protection ?

5,040件の閲覧回数
Max_Arrow
Contributor I
Hello all, I would like to know if there is any level of the code protection because I can't erase the memory after that I've protected it. Anybody knows where I configure this?

--
Alban Edit: FSL Part Number must figure in Message Subject line.

 


Message Edited by Alban on 2007-09-03 09:39 PM
ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,051件の閲覧回数
Marcia
Contributor I
Hi Max_Arrow,
 
Please help us by telling us what ColdFire device you are using, and on what board. Is it a Freescale EVB, or your own target. What flash - internal or external to the device.
 
Bye for now,
 
Marcia
0 件の賞賛
返信

3,051件の閲覧回数
Max_Arrow
Contributor I
Hello Marcia,
I'm using the internal Flash of the MCF52233 in my target board. I've used the M52233DEMO as the reference board.
Thank you
 
0 件の賞賛
返信

3,051件の閲覧回数
blackjack
Contributor I

Hello Max_Arrow,

                            Did you fixed your problem. if it is then could share your solution couse i have the same problem as yours.

 

 

Thanks

blackjack

0 件の賞賛
返信

3,051件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

If the security is enabled it can not be reversed using BDM. A chip erase via the EZport is the only way to unsecure the part (if it doesn't run software that can do thsi when commanded) - this needs an EZport module to be used or another system connected via SPI with the approriate commands.

 

See the following: https://community.freescale.com/message/38162#38162

 

Regards

 

Mark

 

0 件の賞賛
返信

3,051件の閲覧回数
Marcia
Contributor I
Hi Max_Arrow,
 
Thanks for updating the post with the device. That helps a lot.
 
Your board has the flash secured.
Did the information in the device Reference Manual, Version 4.0, page 17-31 (pdf page 273) not help? A bulk erase followed by a blank check should be sufficient to unsecure your device.
 
Bye for now,
 
Marcia
0 件の賞賛
返信

3,051件の閲覧回数
a_yelm
Contributor I
Hi Macia,
 
I'm in the same spot as Max_Arrow (I think), but I would like to be able to erase/unsecure the internal flash of the MCF52233 using the CodeWarrior Flash Program Utility (from Tools->Flash Programmer menu). It's been working fine up to the point where I enabled the chip secure feature. Now the flash is not reachable for me. Perhaps its just a matter of using the correct .cfg file for target initialization(?).
 
Bye,
a_yelm
0 件の賞賛
返信