MCF52223 bsp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52223 bsp

3,986件の閲覧回数
michele_darold
Contributor I
    Hi, is available a bsp for MCF52223 mcu?

    Regards

Michele Da Rold
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,391件の閲覧回数
RickN
Contributor I
Hi Michele,
 
   There is free USB Stack Software for the MCF5222x family of ColdFire Microcontrollers with USB 2.0 Host/Device/OnTheGo interface.  This software was written by CMX Systems, is provided in source code that can be built with CodeWarrior for ColdFire v6.4.  It is called the CMX_USB-Lite stack, and can be downloaded from the Freescale website:
 
 
   There are other choices for operating system software that will run on the MCF5222x, including a new port of uTasker (www.uTasker.com).  
 
    Thanks,
 
       Rick
0 件の賞賛
返信

2,391件の閲覧回数
RickN
Contributor I
Hi,
 
    Check out CodeSourcery for the GNU tools:  http://www.codesourcery.com/gnu_toolchains/coldfire
 
    I believe uTasker now supports the MCF52223 family of MCUs with integrated USB 2.0 in addition to the MCF5223x MCUs with integrated 10/100 BaseT Etherenet.
 
   Thanks,
 
      Rick
0 件の賞賛
返信

2,391件の閲覧回数
michele_darold
Contributor I
Ok, I'll check.

Thank you for your help

Michele Da Rold
0 件の賞賛
返信

2,391件の閲覧回数
michele_darold
Contributor I
ok, for the usb stack I have already download and used it,

my question is about the availabilty of a gnu toolchain that support MCF 52223 mcu from freescale, I have see uTasker but I think it only support MCF5223x that isn't my mcu or I'm wrong?

Regards
0 件の賞賛
返信