MCF52223 ADC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52223 ADC

1,882件の閲覧回数
Archaiwy
Contributor I
Hello everybody,
When i use mcf52223 adc to do my work, i noticed that the "MCF52223 ColdFire® Integrated Microcontroller Reference Manual" page 25-33 tells the ADC clock is gated by ADC bit of SIM_PCE register of SIM module. But I can not find the description on SIM_PCE register. Is it an error or useless register. Does it affect the ADC operation?
 
Thanks millions on any hints
best regards,
ラベル(1)
0 件の賞賛
返信
1 返信

1,004件の閲覧回数
RichTestardi
Senior Contributor II
From other Freescale manuals, I believe the register being described is:

Finally, the SIM_PCE register contains a bit per peripheral to enable clocking to that peripheral. This is useful for power management. These controls are referenced in peripheral-related restrictions later in this document.

Which would actually be the CDADC bit of PPMRH in the 52223 (section 6.2.1).  The clock is enabled (i.e., not disabled) by default.
 
This (documentation error) is also speculated here:
 
 
0 件の賞賛
返信