MCF5221X debugger / programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5221X debugger / programmer

1,434件の閲覧回数
gaminn
Contributor IV

Hello,

I bought this TBLCF board http://www.cncgeeker.com/index.php?main_page=product_info&cPath=7_4&products_id=9&zenid=092a0a87458f... and I would like to program my MCF52213 MCU. As far as now I noticed that my MCU is not in the supported list of the board.

 

I tried to use the debugger to program my MCU but no success. I can see some activity on DSI pin (two square waves) and DSCLK pin (clocks, 120 kHz approx.) when I push Debug button in CodeWarrior IDE (v 7.2). But no activity on DSO pin. I get "can't connect" message in CodeWarrior. The MCU is powered by 3.3 V.

 

 Is there anyone who uses TBLCF together with MCF5221X and can give me some suggestion how to fix my problem?

 

Thank you

 

Martin

ラベル(1)
0 件の賞賛
返信
1 返信

1,149件の閲覧回数
TomE
Specialist II

Read through to the end of the "TBLCF-open-source-debugging-cable" thread that is anchored to the top of this forum.

 

0 件の賞賛
返信