MCF52213 RSTO stays low

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52213 RSTO stays low

ソリューションへジャンプ
2,314件の閲覧回数
gaminn
Contributor IV

Hello,

I have newly bought (never programmed) MCF52213 and when I turn VDD on, RSTO pin stays low all the time. No other pins are connected, only VDD and VSS. There are two 4.7 uF capacitors between VDD and VSS and 32 kHz crystal (and 18 pf caps and 1 Mohm resistor) on my evaluation board. I tried it with 2 pieces of MCF52213 - it is the same.

 

RSTO pin is not short-circuited to VSS or any other pin. RSTI pin is high. Supply voltage is 3.3V, rising edge of VDD lasts 17 us.

 

Here is an image of turning MCF52213 on. You can see, that there is peak on RSTO like the MCU tries to rise up RSTO.

 

.Turning on MCF52213

 

Hope somebody can give me a suggestion.

 

Thank you

 

Martin

ラベル(1)
0 件の賞賛
返信
1 解決策
1,799件の閲覧回数
pgo
Senior Contributor V

Dear Martin,

 

Looking at the datasheet for the chip it would appear that a 32kHz crystal is not supported (1-48MHz only - I think - this detail hard to find!)

 

There is also some requirements for CLKMOD0/1 and resistors on XTAL - The details depend on the package being used.

 

For reference I've attached the schematic for a minimal circuit I have used.  Note- this circuit uses a fundamental-mode 48MHz crystal which tends to be scarce.  Most are 2nd overtone and unsuitable.  I forget if a lower frequency crystal can be used with the USB functionality.

 

bye

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,799件の閲覧回数
gaminn
Contributor IV

Dear pgo,

really thank you for your help. Now everything is ok. I am a newbie to CF V2 - I didn"t know I have to set several pins (EZPCS, TEST, CLKMOD, XTAL) low or high. It"s not like HCS08 or CF V1 where you connect VDD and VSS and it runs. Thank you very much.

 

Martin

0 件の賞賛
返信
1,800件の閲覧回数
pgo
Senior Contributor V

Dear Martin,

 

Looking at the datasheet for the chip it would appear that a 32kHz crystal is not supported (1-48MHz only - I think - this detail hard to find!)

 

There is also some requirements for CLKMOD0/1 and resistors on XTAL - The details depend on the package being used.

 

For reference I've attached the schematic for a minimal circuit I have used.  Note- this circuit uses a fundamental-mode 48MHz crystal which tends to be scarce.  Most are 2nd overtone and unsuitable.  I forget if a lower frequency crystal can be used with the USB functionality.

 

bye

0 件の賞賛
返信