MCF52211 QSPI SD Card Reader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF52211 QSPI SD Card Reader

1,961 次查看
junkers13
Contributor I

Hi, I'm in the processes of determining if I can use the QSPI on the MCF52211 to write to an SD card using an SD card reader breakout board.  I have the MCF5221 demo board and see the QSPI can be accessed via pins on J1.  I'm sure I will have more questions, but wanted to verify that it was possible. 

 

Thank you

标签 (1)
0 项奖励
回复
2 回复数

942 次查看
bluehacker
Contributor III
I think you can. SD card has SPI mode
0 项奖励
回复

942 次查看
junkers13
Contributor I

Better yet, and I'm just shooting this out there, does anyone know of any kind of dev kit or hardware which can write to some sort of NAND flash memory?  My idea doesn't require mobility so instead of using an SD card I'd like to use flash memory or eeprom.  The largest assessable memory I could find on a microcontroller was around 2MB, I would need closer to 256MB.

 

Thanks to anyone can point me in the right direction.

Message Edited by joey c on 2009-06-19 08:44 AM
Message Edited by joey c on 2009-06-19 08:46 AM
0 项奖励
回复