MCF5213 port pull-ups

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5213 port pull-ups

1,803件の閲覧回数
life_user
Contributor I
 In the users manual for the MCF5213 there is no mention of pull-up resistors for port TC pins (PTC[0] thru PTC[3]). However, if these four are lines are defined as general purpose inputs these pins are acting as if there are approximately 30k pull-up resistors internally.
 Are there internal pull-ups on port TC?
ラベル(1)
0 件の賞賛
返信
1 返信

1,060件の閲覧回数
Nouchi
Senior Contributor II
Hello,

I think there's pull-up on Port TC, because in the MCF5213EC datasheet, Table 3 P18 Pull-up/pull-down column says, "2 All signals have a pull-up in GPIO mode".
In table 26, there's a parameter (Iapu) which specify the Weak Internal Pull Up Device Current, tested at VIL Max.

Emmanuel
0 件の賞賛
返信