MCF5213 external clock and PWM issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF5213 external clock and PWM issue

1,498 Views
pmrshudson
Contributor I
I'm using a MCF5213 with an external master clock. I'm also using one of the 5213 PWM outputs to drive a MOSFET to control the speed of a fan. If I stop the master clock, I notice that the PWM will continue to run. I'd like the PWM to stop when the master clocks stops. Why does the PWM continue to run, and how can I get it to stop when the master clock is halted?
Labels (1)
0 Kudos
Reply
1 Reply

943 Views
RichTestardi
Senior Contributor II

When you stop the external clock (or even before), can you examine SYNSR and see where the MCU thinks the clock is coming from?  Is EXTOSC always set, and OCOSC/CRYOSC clear?  There is loss of clock circuitry (SYNCR->LOCEN), to automatically switch clocks or reset the MCU, but the data sheet seems to imply is disabled when running off an external clock.  See Reference Manual section 6.8.4.8.

 

0 Kudos
Reply