MCF5213 ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF5213 ADC

4,221 Views
Vijaya
Contributor I
Hi,
I want to know about the type of ADC in MCF5213
Thanks.
 
Labels (1)
0 Kudos
Reply
1 Reply

2,888 Views
mpeters
Contributor I
Here are the main features of the AtoD converter on the MCF5213:

The analog-to-digital converter (ADC) consists of two separate and complete ADCs, each with their own
sample and hold circuits. The converters share a common voltage reference and common digital control
module.

The ADC’s characteristics include the following:
• 12-bit resolution
• Maximum ADC clock frequency of 5.0 MHz, 200ns period
• Sampling rate up to 1.66 million samples per second1
• Single conversion time of 8.5 ADC clock cycles (8.5 × 200ns = 1.7µs)
• Additional conversion time of 6 ADC clock cycles (6 × 200ns = 1.2µs)
• Eight conversions in 26.5 ADC clocks (26.5×200ns = 5.3µs) using simultaneous mode
• Ability to simultaneously sample and hold 2 inputs
• Ability to sequentially scan and store up to 8 measurements
• Internal multiplex to select two of 8 inputs
• Power savings modes allow automatic shutdown/startup of all or part of ADC
• Those inputs not selected tolerate injected/sourced current without affecting ADC performance,
supporting operation in noisy industrial environments.
• Optional interrupts at the end of a scan, if an out-of-range limit is exceeded (high or low), or at zero
crossing
• Optional sample correction by subtracting a pre-programmed offset value
• Signed or unsigned result
• Single ended or differential inputs for all input pins with support for an arbitrary mix of input types

More information on the A/D converter can be found in the MCF5213 user's manual. Here's the link:
http://www.freescale.com/files/32bit/doc/ref_manual/MCF5213RM.pdf

regards,
mpeters
0 Kudos
Reply