MCF51QE128 - CPU speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF51QE128 - CPU speed

2,642 Views
Richard777
Contributor I
Hi, I'm a MCF51QE128 beginner, I will be select a 16 Mhz Xtal like external oscilator, and I will be select the internal bus frecuency to 24 Mhz, with this values the frecuency of Core is 48 Mhz ?
Thanks in advance

--
Alban Edit: Please always include FSL Part Number in Message Subject line.
http://forums.freescale.com/freescale/board/message?board.id=FORUMUSE&message.id=865



Message Edited by Alban on 2007-10-15 11:57 AM
Labels (1)
0 Kudos
Reply
2 Replies

1,327 Views
UK_CF_FAE
NXP Employee
NXP Employee
Hi Richard,
 
On the MCF51QE128 the instruction clock is the same frequency as the output from the ICS, and the bus clock (peripherals etc) is divided by 2.
 
Instruction clock = ICSCLK
Bus Clock = ICSCLK / 2
 
Device Reference Manual, PDF page 24. Figure 1-3
 
So, yes, if you use the 16MHz crystal, set the FLL to generate 48MHz, then the core will run at 48MHz and the peripherals at 24MHz.
 
I reckon
ICSC1_CLKS = 00
ICSC1_RDIV =  100
ICSC1_IREFS = 0
 
ICSC2_RANGE = 1
 
ICSSC_DRS = 10 (FLL factor is 1536)
 
This is going to give 48MHz exactly. Good luck
 
Mark
0 Kudos
Reply

1,327 Views
Richard777
Contributor I
Alban sorry for my mistake and Mark a lot of thanks for your explanation :manvery-happy:
 
Bye
0 Kudos
Reply