MCF51JM128 Assembly Questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF51JM128 Assembly Questions

1,907 Views
RRVIZ
Contributor I
Hi everyone,
 
I've been trying to analyse some routines in a program written in C language with the Disassemble option in CW for Microcontrollers V6.2 (the trial version), to see the assembly instructions, but I've got some doubts:
 
1. The .dump window for my source file has this line:
 
;Address        ObjectCode  Label  Opcode   Operands              Comment
0x0000000E  0x600A                     bra.s        *+12                      ; 0x0000001a
 
From which I understand that will set the Program Counter to the address of the instruction + 2 + 12 (0x00000E + 2 + 12 = 0x00001C) and not to 0x00001A as the comment says.
 
But if we look at the machine code, it is 0x600A, which means that the displacement is 0x0A, a 10 in decimal, and that would set the PC to 0x00001A as it suposeddly must do. So I want to know why the displacement at the Object Code is different to that of the assembly operand.
 
Here is the description for BRA, as it says in the Coldfire Family Programmer Reference Manual:
"Description: Program execution continues at location (PC) + displacement. Branches can be forward with a positive displacement, or backward with a negative displacement. The PC contains the address of the instruction word of the BRA instruction plus two."
 
Probably I'm misunderstanding something, so please explain me why this happens. Besides, I don't know what that .s in the instruction stands for (I only knew there was .b, .w and .l) and there may lie the answer, but I can't find what it means even in the Coldfire Reference.
 
 
2.  On the same disassembly there is this line:
 
;Address        ObjectCode  Label  Opcode   Operands              Comment
0x0000001C  0x63F2                     bls.s        *-12                       ; 0x00000010
 
Which would make the program counter point after the previous command I showed you. The function of this line is very clear, but again, I don't know what the .s is for and also I can't find the instruction BLS neither in the Colfire RM, nor in the MCFJM51 RM. So I would like to know what they mean.
 
3. I would like you to provide me some references to understand .dump disassembly files better, as there are many sections I don't understand and they seem to have very useful information.
 
 
Thanks in advance.
Labels (1)
0 Kudos
Reply
1 Reply

1,140 Views
kef
Specialist I
Regarding disassembly window only:
 
In bra.s, ".s" probably stands for signed, I guess.
 
Asterisk * means not current PC, but an address of a label to the left of instruction. Just like we can use it in motorola assemblers:
 
   bra  *+12
 
and
 
 label:  bra  label+12
 
are the same.
 
 
0 Kudos
Reply