MCF51JM Drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF51JM Drivers

2,000 Views
a_sangros
Contributor I

Hi!

Using this micro in Windows 7 and 8 it's not possible to be recognized. Under Windows 10 is okey. I haven't found drivers for Windows 7 and 8. I need your help.

Thanks in advance.

0 Kudos
Reply
3 Replies

1,894 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I think you are using MCF51JM for USB device application.

Please check if this issue also happened at [Flexis JM Demonstration Board].

Please check MCF51JM USB circuit design and USB communication signal quality.

Thank you for the attention.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,894 Views
a_sangros
Contributor I

Hi, @Hui_Ma 

Thanks for your answer. I've written an inf file to link the sys file of the driver and it works! Solved in w7 64 bits. I'll test it in other versions.

Best regards,

 Arturo

0 Kudos
Reply

1,894 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Arturo,

Nice to hear the issue had been resolved. Thanks for the info.

best regards,

Mike

0 Kudos
Reply