MCF51CN128 and external clocking voltage level

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF51CN128 and external clocking voltage level

857 次查看
KSlava
Contributor I

I'm a little confused after browsing datasheet and reference manual. I couldn't find information about the voltage level of external clock for the cpu. In my current desigh there are many ICs required clocking, so I decided to use programmable  PLL-based synthesizer with multiple outputs, like CDCE925, CDCE949. 

Do I have to use VDD level clock ? I have a lot of experience with ARM based MCUs, and a lot of them require 1.8V level external clock signal. There is no information regarding the external clock voltage level in the datasheets exposed on the web site.

标签 (1)
0 项奖励
回复
1 回复

710 次查看
JimDon
Senior Contributor III

If you read the Data Sheet there is a specification for all digital inputs.

 

P Input high voltageall digital inputs

VIH VDD > 2.7 V  0.70 x VDD   VDD > 1.8 V   0.85 x VDD 

Data Sheet

0 项奖励
回复