MCF 5485 Assembly instruction reference manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF 5485 Assembly instruction reference manual

1,689 Views
Sethu123
Contributor I

Hi,

 

Could you please provide me data sheet of assembly instructions with sample programs for MCF5485 processor.

 

Thanks,

Sethu

Labels (1)
0 Kudos
Reply
3 Replies

1,429 Views
J2MEJediMaster
Specialist I

Sorry, the best I can do is provide you a copy of the V4 Core instruction manual, since the MCF5485 is a V4 part. That took some work to track down. If there are any assembly examples, you would find them with the tools that you are developing with.

 

---Tom

0 Kudos
Reply

1,429 Views
aersek
Contributor I

http://www.freescale.com/files/dsp/doc/ref_manual/CFPRM.pdf

 

Here are all ColdFire instructions. V4 core supports ISA_A, ISA_B and ISA_C instructions.

0 Kudos
Reply

1,429 Views
TomE
Specialist II

> CFPRM.pdf

 

That provides the Assembly instructions as requested.

 

The other link is very valuable.

 

J2MEJediMaster has managed to locate the "Long Lost Core Reference Manual for the CF4".

 

This lists a lot more essential information about the CF4 core than just the assembly instructions. The stuff needed to put operating systems on it and so on.

 

But it is not available from the Freescale web site; they don't seem to offer all the necessary documentation for the CF4 to the public.

 

To take local copies of it from this thread while you can.

 

And if anyone has a non-broken copy of the CF3 Core manual, please let me know.

 

Tom

 

0 Kudos
Reply