MC68332ACEH20 shortage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC68332ACEH20 shortage

Jump to solution
5,827 Views
AlexandroSantos
Contributor I

Hello,

Our PCB manufacturer has reported us shortage on the processor MC68332ACEH20, I see as drop in replacement the processor MC68332ACEH25.

It seems to me that the only difference is that MC68332ACEH25 has capability to run faster than MC68332ACEH20.

I'm going to go deep into the Datasheet and user manual, but if someone may confirm that both processors will work same with the same code I really appreciate. 

Regards.

0 Kudos
Reply
1 Solution
5,813 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Customer can use MC68332ACEH25 to replace MC68332ACEH20 chip without any software & hardware modification.  Thanks for the attention.

best regards,

Mike

 

View solution in original post

0 Kudos
Reply
5 Replies
5,814 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Customer can use MC68332ACEH25 to replace MC68332ACEH20 chip without any software & hardware modification.  Thanks for the attention.

best regards,

Mike

 

0 Kudos
Reply
4,743 Views
patriot75
Contributor I

Mike,

I have an MC68332ACEH16 design where I installed a MC68332ACEH25. The component is not able to lock onto the external 32.768KHz clock.  Nothing has changed other than swapping devices. FW controls the clock divisor. As a test, I can insert an external reference in place of the crystal to allow it to work. The intent is for the -25 to be a drop in replacement.
Is this expected?

 

0 Kudos
Reply
5,794 Views
AlexandroSantos
Contributor I

Hi Mike @Hui_Ma ,

We tried to get stock of MC68332ACEH25, but it is no longer available. 

There is another option available which is: MC68332AVEH25.

Is that an option that doesn't require neither software nor hardware changes?.

Regards.

 

0 Kudos
Reply
4,714 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

The only difference of MC68332ACEH25 vs. MC68332AVEH25 is operation temperature.

There with no hardware and software change requirement.

Please refer below picture about the operation temp. range.

Hui_Ma_0-1667195954450.jpeg

B.R.

Mike

0 Kudos
Reply
5,782 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer below 68K product naming rule.

Hui_Ma_0-1644633801339.jpeg

 

The only difference of MC68332AVEH25 vs. MC68332ACEH25 is operation temperature.

There does not need any hardware and software change. Thanks.

Mike

 

0 Kudos
Reply