MC68332ACEH20 shortage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC68332ACEH20 shortage

ソリューションへジャンプ
5,829件の閲覧回数
AlexandroSantos
Contributor I

Hello,

Our PCB manufacturer has reported us shortage on the processor MC68332ACEH20, I see as drop in replacement the processor MC68332ACEH25.

It seems to me that the only difference is that MC68332ACEH25 has capability to run faster than MC68332ACEH20.

I'm going to go deep into the Datasheet and user manual, but if someone may confirm that both processors will work same with the same code I really appreciate. 

Regards.

0 件の賞賛
返信
1 解決策
5,815件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Customer can use MC68332ACEH25 to replace MC68332ACEH20 chip without any software & hardware modification.  Thanks for the attention.

best regards,

Mike

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
5,816件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Customer can use MC68332ACEH25 to replace MC68332ACEH20 chip without any software & hardware modification.  Thanks for the attention.

best regards,

Mike

 

0 件の賞賛
返信
4,745件の閲覧回数
patriot75
Contributor I

Mike,

I have an MC68332ACEH16 design where I installed a MC68332ACEH25. The component is not able to lock onto the external 32.768KHz clock.  Nothing has changed other than swapping devices. FW controls the clock divisor. As a test, I can insert an external reference in place of the crystal to allow it to work. The intent is for the -25 to be a drop in replacement.
Is this expected?

 

0 件の賞賛
返信
5,796件の閲覧回数
AlexandroSantos
Contributor I

Hi Mike @Hui_Ma ,

We tried to get stock of MC68332ACEH25, but it is no longer available. 

There is another option available which is: MC68332AVEH25.

Is that an option that doesn't require neither software nor hardware changes?.

Regards.

 

0 件の賞賛
返信
4,716件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

The only difference of MC68332ACEH25 vs. MC68332AVEH25 is operation temperature.

There with no hardware and software change requirement.

Please refer below picture about the operation temp. range.

Hui_Ma_0-1667195954450.jpeg

B.R.

Mike

0 件の賞賛
返信
5,784件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer below 68K product naming rule.

Hui_Ma_0-1644633801339.jpeg

 

The only difference of MC68332AVEH25 vs. MC68332ACEH25 is operation temperature.

There does not need any hardware and software change. Thanks.

Mike

 

0 件の賞賛
返信