M5485EVB Running Linux 2.6.25: Any Freescaler, CAN Locks OS!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M5485EVB Running Linux 2.6.25: Any Freescaler, CAN Locks OS!

2,962 Views
jkimble
Contributor III

Running the 2.6.25 kernel on the M5485EVB board, following the instructions from the "Getting Started", area of the BSP install.

 

I can bring both CAN's up with ifconfig. However "cantest can0  123#DEADBEEF" locks the OS up tight. There are several of us having trouble with this (some posted some not). Is there anyone that can give us some insight into this issue. CAN's a pretty important means of communication in the embedded world so I would think this is just going to get more critical. I've fought the problem for a while on some custom hardware but I finally just went back to the evaluation board and, lo and behold, it's doing the same thing.

 

Any help much appreciated.

Labels (1)
0 Kudos
Reply
3 Replies

2,037 Views
kmahan
Contributor I

It would help if someone called Freescale support and logged a bug.

 

So you know -- 

 

The Linux work is being transitioned from the US to China.  The US office where this work was done (in Utah) has been closed and the engineers laid off.

0 Kudos
Reply

2,037 Views
jkimble
Contributor III

I'll phone in a bug report.

 

Sad to hear that but thanks for the info...

0 Kudos
Reply

2,037 Views
J2MEJediMaster
Specialist I
Or you can file a service request that reports the problem using this on-line page.
0 Kudos
Reply