M54455EVB with Rev. 1 silicon - will Linux 2.6.29 work properly?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M54455EVB with Rev. 1 silicon - will Linux 2.6.29 work properly?

Jump to solution
2,506 Views
dmarks_ls
Senior Contributor II

Right now I'm working through a https://community.freescale.com/message/89566#89566 issue, and in the course of it, I recalled a passage from the M54455EVB BSP User's Manual, Rev 1.3, page 3-1:

 

This BSP is known to work on the following board(s) revision(s):

  • Baseboard: M54455EVB Rev D
  • CPU: M54455 Rev 2

Not knowing exactly how to identify the silicon revision (unsure if "Freescale MCF54455 (Mask:48 Version:1)" in U-Boot means Rev 1 silicon), I Googled and found the chip errata document, which shows that Rev 1 is marked "1M22H" and Rev 2 is "2M22H".

 

So I checked my (newly acquired) M54455EVB, and while the sticker on the board says "Rev. D", the chip itself is marked "1M22H", meaning that I've got Rev 1 silicon.

 

Do I have any hope of using the new(ish) Sep-2010 LTIB with Kernel 2.6.29 with this Rev 1 silicon, or do I need to ship my M54455EVB mainboard off for BGA rework to get Rev 2 silicon put on there?  Has anyone had any issues (or heck, any success) with running the 20100919 LTIB on an M54455EVB with Rev 1 silicon?

Labels (1)
0 Kudos
Reply
1 Solution
2,190 Views
J2MEJediMaster
Specialist I

I would file an on-line service request on this. It would accomplish several things:

 

1) Make the engineers aware of the work-around

2) They might have information as to an acutal solution and can pass that back to you,

3) Provide an opportunity to update the documentation.

 

While we do try to solve problems in these forums (and many thanks to everyone who contributes), sometimes it is best to file a service request to get the issue logged into our database and looked at.

 

---Tom

View solution in original post

0 Kudos
Reply
4 Replies
2,190 Views
TomE
Specialist II

The Errata Items current for Mask 1 that are fixed in Mask 2 are:

 

  1. SECF041: Serial Boot with a Crystal
  2. SECF016: SRAM Simultaneous Reads
  3. SECF042: Serial Boot on 256-Pin Devices
  4. SECF034: PLL Loss-of-lock at Large Voltage Differentials

It is unlikely that any of the above could explain the "slow boot".

 

If you don't have a debug pod it might be worth getting one. If you do have a debug pod then using it is the easiest option.

 

Tom

 

0 Kudos
Reply
2,190 Views
dmarks_ls
Senior Contributor II

Well, since I've managed to solve the slow-boot issue (PATA driver going nuts), it seems that Linux 2.6.29 runs fine on Rev 1 silicon.  It would be nice if someone from Freescale could officially verify this and update the BSP user's manual to indicate that Rev 2 silicon is not strictly required.

0 Kudos
Reply
2,190 Views
jkmahan
Contributor III

As I recall (it has been roughly 3 years since I worked on this) the Rev 1 silicon was not produced in volume.  Aside from a few development boards it wasn't made available - and wasn't in any products.  Maybe JWW can correct me?

0 Kudos
Reply
2,191 Views
J2MEJediMaster
Specialist I

I would file an on-line service request on this. It would accomplish several things:

 

1) Make the engineers aware of the work-around

2) They might have information as to an acutal solution and can pass that back to you,

3) Provide an opportunity to update the documentation.

 

While we do try to solve problems in these forums (and many thanks to everyone who contributes), sometimes it is best to file a service request to get the issue logged into our database and looked at.

 

---Tom

0 Kudos
Reply