M5329EVB - Compact Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M5329EVB - Compact Flash

2,647 Views
sygi
Contributor I
Hi Everyone. Is there possibility to mount CF memory under uClinux on the M5329EVB board. I can't find any support for CF memories in the uClinux kernel configuration file (LTIB-20061117). Maybe there is some CF-patch ?. I wondering if there is possibility to direct access trough memory map (somewhere /dev/* ?). Does Anyone can help me ?? Regards.
Labels (1)
0 Kudos
Reply
2 Replies

1,649 Views
AdamS
Contributor I
 
Hello,
 
in fact CF are connected in memory mapped mode on MCF5329evb and MCF5475/85evb. So you are not able to access it in True IDE mode (just like a classic CF/ HDD). You can access it as the memory space only.
 
B.R.  - Adam 
0 Kudos
Reply

1,649 Views
DavidS
NXP Employee
NXP Employee
Hello,
The MCF5329 silicon with mask set 2M29B and older had errata relating to the chip select programmable address hold feature (errata #11 in the MCF5329DE.pdf on the web).
That errata prevented the CF interface from working properly.
The latest silicon mask 3M29B has fixed this errata.  So hopefully with the next release/update of the LTIB BSP for M5329EVB this interface will be supported.
Regards,
David
0 Kudos
Reply