M5227xevb BSP iso issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M5227xevb BSP iso issue

3,344件の閲覧回数
agm
Contributor I
Hi,

I have tried to download and use the BSP for the M52277 evb, but the iso seems to be corrupted, I can't burn it on a CD, or load it with mount.
Did anyone else manage to use the iso file?
Can someone tell me how I can access the first revision of the BSP (as I see, this is the second revision, maybe the first one will work)?

Thank you in advanced for any tips

Best regards, Muntianu Andrei Gabriel
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,277件の閲覧回数
J2MEJediMaster
Specialist I
I have downloaded the image file in question, and confirmed that it does not mount. I have checked with the engineers and yes, there's a problem with the image file. It's being worked on. Sorry, I do not have a delivery date on the fix.

---Tom

0 件の賞賛
返信

2,277件の閲覧回数
agm
Contributor I
Thank you for looking into this matter.

Can you provide a link to the first version of this BSP? Perhaps that image file works.
0 件の賞賛
返信

2,277件の閲覧回数
J2MEJediMaster
Specialist I
I have good news for you. The file has been fixed and the download md5sum confirmed. You can get the fixed file from here:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061033202A9

HTH.

---Tom
0 件の賞賛
返信

2,277件の閲覧回数
agm
Contributor I
Thank you:smileyvery-happy:
0 件の賞賛
返信