M52277EVB dBug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M52277EVB dBug

2,092 Views
ianlovatt
Contributor III

Does anyone know why the M52277EVB dBug project available here does not run from flash?

 

http://www.freescale.com/webapp/sps/download/license.jsp?colCode=M52277EVB_DBUG_SRC&location=null&fs... search&Parent_pageType=from search

 

Both RAM and FLASH targets run when debugging in CW but the program fails to start when the EVB is power cycled away from the debugger. Unless I've missed something fundamental about how the dBug project works I believe it should execute from flash like any other program...

 

Cheers

ian

Labels (1)
0 Kudos
Reply
2 Replies

1,635 Views
cw_weldon
Contributor I

You can diconnect the Multilink and reset the board to see if this brings it up.

0 Kudos
Reply

1,635 Views
ianlovatt
Contributor III

Yes that's what i'm doing, once the board is flashed it should startup after reset without the multilink connected but it doesn't. I know the h/w is fine as other projects startup ok.

0 Kudos
Reply