M52259DEMO schematics?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M52259DEMO schematics?

5,386件の閲覧回数
vier_kuifjes
Senior Contributor I
I have a M52259DEMO board on order at Freescale. Shipping is planned around March 24th, which means that I still have a lot of waiting to do...:smileysad:

In the mean time I'd like to get to know a little more about the board, or better, two boards. I have found the schematic diagram of the MCU board on the Axiom Manufacturing web site, but apparently the schematic of the COM board (the one with the ethernet interface) is not present.

Is there anyone who can provide me with the COM board schematic?

Alternatively, I'm interested in the M52259EVB board schematics also. Maybe if someone can provide me with that?

Thanks in advance.
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,516件の閲覧回数
macl
Senior Contributor I

Hi,

 The schematics are available on the M52259DEMOKIT site under Downloads.  

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=M52259DEMOKIT

 

best of luck,

macl

Message Edited by macl on 2009-02-18 02:53 PM
0 件の賞賛
返信

2,516件の閲覧回数
vier_kuifjes
Senior Contributor I
Thanks!
0 件の賞賛
返信

2,516件の閲覧回数
RichTestardi
Senior Contributor II
Hi Marc,
 
Check your forum mail.
 
(I didn't know if it was appropriate for me to repost someone else's file here.)
 
-- Rich
 


Message Edited by Rich T on 2009-02-14 01:33 PM
0 件の賞賛
返信

2,516件の閲覧回数
vier_kuifjes
Senior Contributor I
Thanks Rich!
0 件の賞賛
返信

2,516件の閲覧回数
RichTestardi
Senior Contributor II
Weird, I tried to send you a file list off the DVD in the forum mail, but the message appears empty when I look at it.  So here it is.  [email protected]
 
D:\>ls -R | cat
.:
AUTORUN.INF
Scripts
WT_2865_Kirin3_DVD.exe
WT_2865_Kirin3_DVD.html
WT_2865_Kirin3_DVD.swf
files
freescale.ico
fscommand
./Scripts:
AC_RunActiveContent.js
./files:
development
documentation
software
./files/development:
M52259DEMOKIT_Quick_Start_Guide.pdf
M52259EVB_Quick_Start_Guide.pdf
MCF5225xCFTCPIP_Lab.pdf
MCF5225x_ColdFire_USB_Lite_Stack_by_CMX_Lab.pdf
MCF5225x_USB_Bootloader_Lab.pdf
MSG_15762_MQX_LABS.pdf
video_freescale
./files/development/video_freescale:
MSG-15712_H.264_For_DVD_081212.flv
Scripts
SteelExternalAll.swf
freescale MQX.swf
freescale_MQX.html
./files/development/video_freescale/Scripts:
AC_RunActiveContent.js
./files/documentation:
AN3779.pdf
M52259DEMOCOM_BOM_B.pdf
M52259DEMOCOM_Sch_B.pdf
M52259DEMOCOM_UG.pdf
M52259DEMOKIT_QSG.pdf
M52259DEMOKIT_Quick_Start_Guide.pdf
M52259DEMOMCU_BOM_B.pdf
M52259DEMOMCU_Sch_B.pdf
M52259DEMOMCU_UG.pdf
M52259EVBUser_Manual.pdf
M52259EVB_BOM.pdf
M52259EVB_QSG.pdf
M52259EVB_Quick_Start_Guide.pdf
M52559EVB_Schematics.pdf
MCF52259_CM.pdf
MCF52259_CMRM.pdf
MCF5225X_FS.pdf
MCF5225x_Fact_Sheet_-LR.pdf
./files/software:
Alvaview_FS.pdf
CodeWarrior_FS.pdf
CodeWarrior_QSG.pdf
EA_MQX_PS.pdf
FSL_MQX_RN.pdf
MSG14204_APFSLR.pdf
MSG14206_APFSLR.pdf
MSG14209_CMXSPFSLR.pdf
MSG14211_MPFSLR.pdf
MSG14214SSP_LR.pdf
MSG15802_ELFSLR.pdf
MicroDigital_CFS.pdf
RTOS_CQSG.pdf
Segger_Partner.pdf
Wittenstein_FSLR.pdf
./fscommand:
CWCF_V7_1_1.exe
CW_ColdFire_7_1_Pro_Eval.exe
ColdFire_TCP_IP_Lite_MCF5225x_by_InterNiche.exe
ColdFire_USB_LITE_Stack_MCF5225x_by_CMX.exe
FSLMQXOS.exe
FreeRTOS_lwIP_MCF52259_CodeWarrior_demo.zip
GHS_Partner.zip
IAR_CF_Kirin3_002.zip
IAR_datasheets.zip
Linux_ELF.bin
M52259EVB_Schematics_OrCAD_Source.dsn
MCF52259_CWD.zip
MCF5225x_SAMPLE_CODE.zip
MCF5225x_USB_BOOTLOADER.zip
Windows_ELF.exe
uC_TCPIP_Example_Projects.zip
0 件の賞賛
返信