M52235EVB Exception vector name: Address Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

M52235EVB Exception vector name: Address Error

5,041 次查看
Evan_Chn
Contributor I
When I run the DEMO project TCPIP stack on the M52235EVB board ,I got a message "Exception vector name:Address Error" in mcf5223_lo.s on the line:move.1 #__SRAM,d0,what's wrong ?
thanks
标签 (1)
0 项奖励
回复
6 回复数

2,474 次查看
DrSeuss
Contributor I
It would appear that you have not programmed the code into the device. Use that CW flash programming tool on the title bar. Please see:

http://www.freescale.com/coldfireseminars

for a walk though.

 

Alban corrected link

Message Edited by Alban on 2007-02-09 11:27 AM

0 项奖励
回复

2,474 次查看
Evan_Chn
Contributor I
thanks.After I programmed it into the flash with CF Flasher,it runs with no errors 
0 项奖励
回复

2,474 次查看
Ale
Contributor I
I have the same problem, but the link previously postend don't work!
 
Can I have a new link??
 
 
0 项奖励
回复

2,474 次查看
Alban
Senior Contributor II
Hello,
 
I have corrected the link in the previous post.
it was Cold and not Code in the URL :smileywink:
 
Cheers,
Alban.
0 项奖励
回复

2,474 次查看
Ale
Contributor I
Thanks, it works fine!!!!
0 项奖励
回复

2,474 次查看
Nouchi
Senior Contributor II
0 项奖励
回复