M52235EBV dBUG source or object?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

M52235EBV dBUG source or object?

4,287 次查看
Petter
Contributor II
I'm currently doing development on my M52235EBV board using gcc under Linux. I download and run the SREC files using dBUG. However, I would like to know if my application will run from FLASH using my own ISRs and without the help of dBUG.

This means that I'll have to erase dBUG (or at least parts of it) from the FLASH. I would like to be able to restore dBUG but I can't find the source or an object file for it. Does anybody know where I can obtain a copy of dBUG for the M52235EBV?

My current version is:

dBUG> ver

ColdFire MCF5223 on the M5223EVB
Firmware v4a.1b.1a (Built on Mar 23 2006 11:35:34)
Copyright 2006 Freescale Semiconductor, Inc.
标签 (1)
0 项奖励
回复
5 回复数

2,256 次查看
DrSeuss
Contributor I
Please see attached I'm pretty sure this is ver. 1b.
0 项奖励
回复

2,256 次查看
Petter
Contributor II
FYI: It appears to be the same versjon. After an erase with cfflasher, then verified that the contents was all F's and the board was "dead". Programmed using the uploaded srec file and got:

dBUG> ver

ColdFire MCF5223 on the M5223EVB
Firmware v4a.1b.1a (Built on Mar 23 2006 11:35:34)
Copyright 2006 Freescale Semiconductor, Inc.


However, v4a.1b.1a works fine with me.

P.S.
It would be nice if this was included in the kit as well as a dBUG reference manual...
0 项奖励
回复

2,256 次查看
aalonso
Contributor I
Hi, I’m trying to switch to Linux for my develop environment,
and at the current time I only have a M52233DEMO board,
my question is:
Can I use this dBUG s19 for debugging in my board??
And do I have to flashed on a specific address location????
Thanks =]
0 项奖励
回复

2,256 次查看
Harjit
Contributor II
Did you find/get the source for dBUG for the M52233?
0 项奖励
回复

2,256 次查看
Petter
Contributor II
Thanks!
0 项奖励
回复