M52235 Pinout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M52235 Pinout

3,632 Views
AwfulKanawful
Contributor I
Which document lists the correct pinout for the MCF52235 QFP112: the Reference Manual or the Evaluation Board schematic?

The pins in question are the VSSA, VRH, and VRL. The EVB schematic lists the pins as:
VSSA: 96
VRL: 95
VRH: 94

The ref manual lists:
VSSA: 94
VRL: 96
VRH: 95

Or is this a difference between the MCF52235 and PCF52235? (seems unlikely)

Thanks
Labels (1)
0 Kudos
Reply
1 Reply

1,277 Views
DrSeuss
Contributor I
The EVB schematic is correct the manual is being updated.
0 Kudos
Reply