M52233DEMO Free (open source) need help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M52233DEMO Free (open source) need help

7,136 Views
digit
Contributor I
I'm looking for free (open-source) IDE, toolchain for M52233DEMO board.  M52233DEMO board include MCF52233 + P&E Micro USB BDM on a single board.
 
I have some success building .elf with CodeSourcery toolchain and loading/debugging in RAM with GDB + P&E Micro stub.
 
Is it possible to load in flash using CodeSourcery GDB ?  For now I use CFFlasher to load in flash, the problem is that I can't find how to use CFFlasher from makefile (command line), it look like a freaking non scriptable GUI apps (I'm I wrong ?).
Labels (1)
0 Kudos
Reply
8 Replies

3,594 Views
oed
Contributor I
Try from cmd:

cfflasher -t M52233EVB -p exampe.elf -s -bdm PE_USB_ML

I don't know how to change de USB speed, for this reason I can't used the cfflash :smileysad:, howerer you don't need change USB speed and this command it's ok.
0 Kudos
Reply

3,594 Views
digit
Contributor I
No luck with cfflasher CLI interface...
 
Can't find email contact anywhere is cfflasher for bug report.
 
If someone here have contact @ freescale please forward attached Bug report
 
Message Edited by t.dowe on 2009-09-02 05:04 PM
0 Kudos
Reply

3,594 Views
RuiFaria
Contributor III

hi digit,

 

I am having the same problem than you, i can't program my M52259 by command-line but it is okay using GUI.

 

Did you find a solution for your problem? which was the solution?

 

Thanks.

 

Best regards,

Rui Faria

0 Kudos
Reply

3,594 Views
Zorrillo
Contributor I
There is indeed a bug on CF flasher, however, you still need to open a Service Request. You can do it mailing to [email protected] in case the web is still failing, otherwise will be hard to provide status of the problem.
0 Kudos
Reply

3,594 Views
digit
Contributor I
From freescale:
 
Code:
we would not be able to accommodate your requested change.We have verified that the CLI does not fully function. There are noplans at this time to correct this. You will have to use the GUI, orpurchase a tools for your needs. (P&E makes a CLI for ColdFire)
 
 
0 Kudos
Reply

3,594 Views
J2MEJediMaster
Specialist I
Go to the support section of this Web site (use the Support link at the top of this page), then follow the Request help (online) link to submit a SR (service request) on this.

---Tom
0 Kudos
Reply

3,594 Views
digit
Contributor I
That is for sure a great tool :smileymad:
 
How do I submit bug report on bug report system ?
 
Code:
Unexpected Error We are unable to process your Service Request because of an Unexpected error. Please go back and try again. Please accept our apologies for any inconvenience this may cause. In case of any difficulty, you may access Freescale's Customer Support at one of the following numbers:    Americas: 1-800-521-6274 6AM-5PM Mountain Standard Time   Asia: +852-2666-8307 8AM-6PM Hong Kong   Japan: 0120-191-014 8AM-5PM Tokyo   Europe: +49-89-92103-559 9AM-5PM Munich    Or you can contact us by email at [email protected]   Regards,Freescale Semiconductor Customer Support 

 

Message Edited by digit on 2006-11-2805:21 PM

0 Kudos
Reply

3,594 Views
J2MEJediMaster
Specialist I
Well, it shouldn't doing that. :smileysad:

I have forwarded your problem manually.

I apologize for the trouble.

---Tom
0 Kudos
Reply