M52233 Starter developer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M52233 Starter developer

3,304件の閲覧回数
siliciuro
Contributor I
Hi I'm new to forum.
I have buy M52233 and CodeWarrior Development Kit. I trying to write a simple code tha write a character to RS232 (UART). Can anyone help me with:
1) Example C program
2) Flashing procedure to download the code
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,558件の閲覧回数
Jaux
Contributor I
You might want to consider using embedded Forth... ( www.forth.com) There is a demo version available for the M5223x

I use it across all the Freescale processors and the learning time, development time and deploy is fast, simple and highly effective.
0 件の賞賛
返信

1,558件の閲覧回数
mjbcswitzerland
Specialist V
Hi Siliciuro
 
Go to http://www.utasker.com/ where you can find a tutorial (on the documents page) including how to program the FLASH using CodeWarrior and also the Freescale CF utility.
 
You can also find a link to an online M52233 and an Srec file which can be loaded to your own board demonstrating a web server with dynamic page support, FTP, TELNET, SMTP, and UARTs plus various other stuff. (It matches the tutorial so all instructions are there).
 
On the uTasker page you can read about the simple licensing conditions for the uTasker, which is free for non-commerial work (education, hobby, etc.) and if you want to receive full project code including a M5223X simulator just return the application form. Like that you can have your own web server application and 3 UARTs up and running at the weekend....
 
Regards
 
Mark Butcher
 
0 件の賞賛
返信