M52233 Starter developer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M52233 Starter developer

3,245 Views
siliciuro
Contributor I
Hi I'm new to forum.
I have buy M52233 and CodeWarrior Development Kit. I trying to write a simple code tha write a character to RS232 (UART). Can anyone help me with:
1) Example C program
2) Flashing procedure to download the code
Labels (1)
0 Kudos
Reply
2 Replies

1,499 Views
Jaux
Contributor I
You might want to consider using embedded Forth... ( www.forth.com) There is a demo version available for the M5223x

I use it across all the Freescale processors and the learning time, development time and deploy is fast, simple and highly effective.
0 Kudos
Reply

1,499 Views
mjbcswitzerland
Specialist V
Hi Siliciuro
 
Go to http://www.utasker.com/ where you can find a tutorial (on the documents page) including how to program the FLASH using CodeWarrior and also the Freescale CF utility.
 
You can also find a link to an online M52233 and an Srec file which can be loaded to your own board demonstrating a web server with dynamic page support, FTP, TELNET, SMTP, and UARTs plus various other stuff. (It matches the tutorial so all instructions are there).
 
On the uTasker page you can read about the simple licensing conditions for the uTasker, which is free for non-commerial work (education, hobby, etc.) and if you want to receive full project code including a M5223X simulator just return the application form. Like that you can have your own web server application and 3 UARTs up and running at the weekend....
 
Regards
 
Mark Butcher
 
0 Kudos
Reply