M52223EVB Relaxation Oscillator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M52223EVB Relaxation Oscillator

1,977件の閲覧回数
soccermike
Contributor I
Using the M52223EVB board, I'm trying to use the on-board relaxation oscillator.  When I configure the jumpers, it appears that my on-board oscillator is running at 14MHz.  Additionally, the Coldwarrior Debugger can't modify the ROCR bits TRIM[9:0].  Since the trim is close to the nominal frequency and all the values read back as 0%, this may be the source of the value.  How do I change he ROCR bits?

I also found that CLKSRC functionality doesn't exactly match Figure 5-1. Clock Module Block Diagram.
The diagram shows both the Reference Clock and the PLL come after the Pre-Divider controlled with CCHR.  Instead, I found (and it makes sense) that the Reference Clock comes directly from the CLKMOD0 mux.

Lastly, this diagram should include how OSCSEL affects the clocks.

Thanks in Advance,

Mike
ラベル(1)
0 件の賞賛
返信
1 返信

1,164件の閲覧回数
macl
Senior Contributor I
Hi Mike,
  If the on-board oscillator is 14MHz, then I suspect it is from a small batch of EVBs that went out with initial samples that didn't have the oscillator trimmed correctly.  I recommend returning the board to the distributor (or Freescale, if you bought it direct) and get a new one.  It is not possible to write to the trim bits.
 
On your recommendations for the clock module block diagram, I will forward your suggestions to the documentation team.  Thanks for the feedback. 
 
Mac
0 件の賞賛
返信