M52223EVB Link error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M52223EVB Link error

10,068件の閲覧回数
schildt
Contributor I
Hi,
I'm using the M52223EVB together with the CW Special edition 5.7.0. I'm having problems when trying to compile my code. I was down to 1 linking error and then added the lcf files and suddenly I had 1001 errors. Almost all errors are are like this:
"Link error : Unexpected relocation R_68K_SDA16: __SDA_BASE not set in file xcp_usb.c"
Followed by:
"Link error : Illegal 16-bit small data area relative reference to symbol '_xcp_daq_dto_buffer_status'
from address 0x20004F0 in section '.text' of file 'xcp_usb.c'.
This type of reference has a range from 4294934528 to 32767 bytes."
I can't find any solution to the problem either in the manuals or on the forum.
What am I doing wrong?
I'm trying to implement the ASAM standard communication "XCP on USB" for communication between the evaluation board and my PC.
 
Thanks in advance!
 
Hakan Schildt
ラベル(1)
0 件の賞賛
返信
13 返答(返信)

5,986件の閲覧回数
cristina_c
Contributor I

Hi,

I am migrating my project from CW 5.7 in a XP windows machine to a CW 7.2 in a  W8 machine. When I try to compile I got exactly the same error reported by schildt :

"Link error : Unexpected relocation R_68K_SDA16: __SDA_BASE not set in file xcp_usb.c"

"Link error : Illegal 16-bit small data area relative reference to symbol '_xcp_daq_dto_buffer_status'
from address 0x20004F0 in section '.text' of file 'xcp_usb.c'.
This type of reference has a range from 4294934528 to 32767 bytes."

I have tried with all the solutions suggested above:

- I have changed in Standard Settings-> Coldfire Processor-> Core Model to Smart (16/32)

- I haved changed the Coldfire Processor" panel for the "use .sdata /.sbss for" area to "All data smaller than" to "0"

- By last I have done Project/Remove Object code to force a rebuilt.


Any of those worked for me. Has someone found another solution?


Thanks a lot in advance!!



0 件の賞賛
返信

5,986件の閲覧回数
carloscuevas
Contributor III

I had this problem opening a CFV1 proyect from CW MCU v6.2 in CW MCU v6.3, I solved it this way:

 

Edit > Standard Settings

then under the target setting panel called Coldfire Processor

change the Core Model to Smart (16/32 bit)

or try other options under that combobox.

0 件の賞賛
返信

5,986件の閲覧回数
paulsky
Contributor II

I had the same errors (hundreds of them) when converting from CW6.2 to 6.3. I changed the setting to Smart(16/32 bit) and it worked. Thanks for making your solution available.

 

 

0 件の賞賛
返信

5,986件の閲覧回数
stv7755
Contributor I

I've tried each of the above mentioned suggestions with no luck. Are there any updates to this issue?

0 件の賞賛
返信

5,986件の閲覧回数
Alexutzu
Contributor I

Hi,

 

Try going to ColdFire Compiler->Processor and clear the textbox near "Use .sdata/.sbiss for..... "

 

Alex

0 件の賞賛
返信

5,986件の閲覧回数
CrasyCat
Specialist III
Hello
 
Which Code Model and Data Model did you activate in the "Coldfire Processor" panel?
Try activating "Far (32 bit)".
 
Does it help?
 
CrasyCat
0 件の賞賛
返信

5,986件の閲覧回数
schildt
Contributor I
Hi,
thanks for the quick response! Both the code and data model are set to "Far (32 bit)". I've also tried using smart and near and neither works.
 
Do I need the linking command files (lcf) from the CMX USB stack?
 
/Hakan
0 件の賞賛
返信

5,986件の閲覧回数
CrasyCat
Specialist III
Hello
 
To get someone investigate the .lcf file issue, I would suggest you to submit a service request.
 
I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.
 
Something else you can try the following:
In the "Coldfire Processor" panel set "All data smaller than" and enter "0" in the group "use .sdata /.sbss for". 
 
CrasyCat
0 件の賞賛
返信

5,986件の閲覧回数
schildt
Contributor I
hi,
 
I tried changing the Coldfire Processor" panel for the "use .sdata /.sbss for" area to "All data smaller than" to "0". But it didn't help so I did the pack and go and submitted a SR.
 
Tanks for your help anyway!
 
/Hakan
0 件の賞賛
返信

5,986件の閲覧回数
SanjayJ
Contributor I
How your problem resolved? I am also facing similar kind of linker problem.
0 件の賞賛
返信

5,986件の閲覧回数
JimDon
Senior Contributor III
I have noticed that when you change the link file, all modules do not always get rebuilt, and I have fixed link error doing this.

Project/Remove Object code to force a rebuilt.

0 件の賞賛
返信

5,986件の閲覧回数
SanjayJ
Contributor I
I have already done this, but problem remains the same.
0 件の賞賛
返信

5,986件の閲覧回数
DRuffer
Contributor I
Has anyone found a solution to this yet?  I just ran into it converting an application from 6.1 to 7.1.
0 件の賞賛
返信