M5221X Bus Frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M5221X Bus Frequency

2,883件の閲覧回数
mjbcswitzerland
Specialist V
Hi All

I am a little confused as to the maximum bus frequency quoted on the M5221X Product Summary Page:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF5221X&nodeId=0162468rH3YTLC00M9544...

The M5221X types are given to have 25MHz to 40MHz maximum bus speed.
In the data sheets and user manual the values of 50MHz to 80MHz are specified.

[As a comparison - the M5222X are specified on the product summary page to have max. bus speed of 80MHz, corresponding to the same value of 80MHz as specified in the data sheet].

Is this an error or a different interpretation?

Regards

Mark

www.uTasker.com


ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,767件の閲覧回数
JimDon
Senior Contributor III
Mark,
Yes, I did notice that. I think the various docs use incorrect terminology. The max. clock rate is 80Mhz, which should be called the System clock, and the (IO) bus clock is system clock/2. So that would mean that the (IO) bus clock is 40 MHz max. At different points they seem to confuse these terms, and possible introduce other terms.  The seem to use "bus clock" to refer to both the CPU (System) bus and the IO bus clock.



0 件の賞賛
返信

1,767件の閲覧回数
SimonMarsden_de
Contributor II
Yes, be careful. This problem affects much of the ColdFire documentation.

You need to treat the term 'System Clock' with caution in any ColdFire manual. It is sometimes used for the bus clock and sometimes for the core clock.

In some of the manuals there is a helpful diagram (usually in the PLL section), which shows the clock routing to all the peripherals. You can use it to check which ones receive a divided-by-two bus clock.


0 件の賞賛
返信

1,767件の閲覧回数
RichTestardi
Senior Contributor II
Hi Mark,
 
Isn't the CPU speed twice the (I/O) bus speed?  Or did I misunderstand totally?  All the peripherals seem to operate that way?
 
-- Rich
 
0 件の賞賛
返信