Low Power Operation on the MCF5213

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Low Power Operation on the MCF5213

5,098件の閲覧回数
Gcoakley
Contributor I

Hello All,

Can anyone provide any assistance on Low Power Operation on the MCF5213?  I believe I have the registers (LPCR, LPICR, PPMRH, and PPMRL) set correctly, but I cannot find the "STOP instruction" mentioned in the "MCF5213 Reference Manual".  Is there sample code available which illustrates Low Power Operation?  Thank you.

gcoakley

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,157件の閲覧回数
Felix
Contributor I
Where did you find it? URL?

TIA
0 件の賞賛
返信

2,157件の閲覧回数
Gcoakley
Contributor I

Here are the links, I found.

http://www.freescale.com/files/32bit/doc/app_note/AN3236.pdf

http://www.freescale.com/files/netcomm/software/app_software/code_examples/MCF5213SC.zip

The code example (power) also requires the following definitions.

#define stop_2700() asm(" stop #0x2700")
#define stop_2600() asm(" stop #0x2600")
#define stop_2500() asm(" stop #0x2500")
#define stop_2400() asm(" stop #0x2400")
#define stop_2300() asm(" stop #0x2300")
#define stop_2200() asm(" stop #0x2200")
#define stop_2100() asm(" stop #0x2100")
#define stop_2000() asm(" stop #0x2000")

-gcoakley

0 件の賞賛
返信

2,157件の閲覧回数
Gcoakley
Contributor I
Ok.  I have found the solution myself.  Thank you Freescale, it only took three days of searching through your confusing website with your poor search engine to find sample code and documentation.
 
gcoakley
0 件の賞賛
返信