Linker error undefined "__sinit__" when converting project from CW 6.3 to 7.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linker error undefined "__sinit__" when converting project from CW 6.3 to 7.2

1,730 Views
rbraisted
Contributor I

I'm trying to migrate to a newer version of the CodeWarrior compiler for ColdFire processors. I had a project that successfully built and linked in the old version. (the good ole days), but fails with the newer version. I saw some messages related to removing obsolete libs during the conversion that i suspect might be related to the problem. Here are some more details:

 

old => CodeWarrior® Development Studio for ColdFire Architectures Version 6.3, Build 14

          IDE Version: 5.7.0 Build 2015

 

new => CodeWarrior Development Studio for ColdFire Architectures Version 7.2, Build 91218.

          IDE Version: 5.9.0 Build 5293

 

when you open the existing .mcp file, CodeWarrior automatically converts to the newer version because of differences in preference panel data between the versions among other things. When i try to build this same project after the auto-conversion happens i get the following linker error.

 

Link Error : Undefined : "__sinit__"

Referenced from "__call_static_initializers" in

Labels (1)
0 Kudos
Reply
1 Reply

1,498 Views
cristina_c
Contributor I

Hi Rober,

I am having a kind of similar problem. How did you fix it?

Thanks!

0 Kudos
Reply