LX2160A Reconstructed Clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LX2160A Reconstructed Clock

2,362 次查看
muhammed_mufeed
Contributor I

Hi Team,

The LX2160A has 2 recovered or reconstructed clock. What is the use of these pins? Can I recover the PTP clock from the serdes via these pins. If possible how to do hardware connections.

0 项奖励
回复
3 回复数

2,234 次查看
muhammed_mufeed
Contributor I

Hi Ufedor,

Then what is the use of these recovered clock. Can I connect this recovered clock to a network synchronizer.

0 项奖励
回复

2,234 次查看
ufedor
NXP Employee
NXP Employee

Excuse me, these are test pins which can be left unconnected if not used for SerDes operation evaluation.

0 项奖励
回复

2,234 次查看
ufedor
NXP Employee
NXP Employee

These are the clocks recovered from SerDes lanes running Ethernet protocols (SGMII, XFI/USXGMII, 25G, etc) on SerDes 1 and 2.

>  Can I recover the PTP clock from the serdes via these pins.

No.

> If possible how to do hardware connections.

These are test pins which can be left unconnected.

0 项奖励
回复