LX2160A Reconstructed Clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LX2160A Reconstructed Clock

2,381件の閲覧回数
muhammed_mufeed
Contributor I

Hi Team,

The LX2160A has 2 recovered or reconstructed clock. What is the use of these pins? Can I recover the PTP clock from the serdes via these pins. If possible how to do hardware connections.

0 件の賞賛
返信
3 返答(返信)

2,253件の閲覧回数
muhammed_mufeed
Contributor I

Hi Ufedor,

Then what is the use of these recovered clock. Can I connect this recovered clock to a network synchronizer.

0 件の賞賛
返信

2,253件の閲覧回数
ufedor
NXP Employee
NXP Employee

Excuse me, these are test pins which can be left unconnected if not used for SerDes operation evaluation.

0 件の賞賛
返信

2,253件の閲覧回数
ufedor
NXP Employee
NXP Employee

These are the clocks recovered from SerDes lanes running Ethernet protocols (SGMII, XFI/USXGMII, 25G, etc) on SerDes 1 and 2.

>  Can I recover the PTP clock from the serdes via these pins.

No.

> If possible how to do hardware connections.

These are test pins which can be left unconnected.

0 件の賞賛
返信