LTIB problem testing network - proxy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB problem testing network - proxy

2,496 Views
raulen
Contributor III
Hello all,
 
I am working with a mcf5484Lite evalutaion board. I downloaded the last revision of ltib for this processor (mcf547x/8x). If I just configure LTIB with prebuilt options, it works perfectly, but If I try to add some packages like gdbserver or expat, the LTIB tries to connect somewhere, but it fails.
My internet connection is located after a proxy. So I guess this is the problem. How should I configure the .ltibrc in order to get it works?
 
Thanks in advance,
Raúl
Labels (1)
0 Kudos
Reply
1 Reply

1,357 Views
MujjuHah
Contributor II

There is configuration file under /ltib folder by name .ltibrc. You can specify the proxy server and port in there.

0 Kudos
Reply