LCDC in M52277EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCDC in M52277EVB

1,801 Views
admin
Specialist II

Hello,

 

I recieve the M52277EVB a few days ago. I can programm the flash, the sdram and execute several examples in the board. The problem I have is the LCDC initialization. I did not find any example code using the LCDC, I try to make it by myself but It does not work... Where can I find an example using LCDC for the M52277? (I´m using Codewarrior v7.1).

 

Thank you very much in advance.

Labels (1)
0 Kudos
Reply
1 Reply

1,202 Views
ianlovatt
Contributor III

There were example projects (eg. m52277evb_photo_album_cw7.mcp) that used the LCDC on the CD that came with our M52277 EVB.

 

ian

0 Kudos
Reply