JM Badge Board Trouble

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JM Badge Board Trouble

ソリューションへジャンプ
2,351件の閲覧回数
Kiwi
Contributor I

Hi,

just got the Flexis JM Badge Board. Connecting it to my Win7 machine has it shown in the Device Manager as a HID Keyboard device and also under Human interface Devices as a USB input device. I have tried to manually update the driver from the Windows7SensorDevKit->Drivers->Binaries->AMD64->SensorBadgeDriver but it fails.

There is another post that describes connecting the board via USB, then hitting E8 twice (http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=7930&query.id=173070#...) , but this totally freaked out my computer.

 

So I am stuck, all the preloaded demos work. Pluggin in via usb then hitting E5 and then E8 allow me to use the touch sensors as buzzer notes. Besides that I got nothing.

 

Any help would be most appreciated,

Kind regards,

Kiwi

ラベル(1)
0 件の賞賛
返信
1 解決策
1,681件の閲覧回数
mnorman
NXP Employee
NXP Employee

Hi, Kiwi,

 

Can you get the USB bootloader mode (mass storage device) to enumerate correctly? 

 

Does this post help?

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=7930#M7930

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,682件の閲覧回数
mnorman
NXP Employee
NXP Employee

Hi, Kiwi,

 

Can you get the USB bootloader mode (mass storage device) to enumerate correctly? 

 

Does this post help?

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=7930#M7930

 

0 件の賞賛
返信
1,681件の閲覧回数
Kiwi
Contributor I

Hi MNorman,

you know I had actually read that post, but didn't get it. So you pointing me back to it, a fresh day, and all is good. My many thanks for such a speedy reply. The board is simply brilliant. Everything I hoped it would be having watched the PDC videos of it.

 

Cheers,

Kiwi

0 件の賞賛
返信