JM Badge Board Contest

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JM Badge Board Contest

9,108 Views
mpeters
Contributor I

The Freescale JM Badge Board Contest is now open for submissions! Enter the contest for your chance to win up to $5000 US dollars.



For contest rules, Badge Board examples, software, ordering instructions, and other information, please go to the JM Badge Board Contest website:

www.canyourbadgedothis.com



Feel free to use this ColdFire forum as a place to ask questions, troubleshoot, and exchange ideas with other JM Badge Board users!

Labels (1)
0 Kudos
Reply
9 Replies

3,554 Views
AndreiBoeru
Contributor I
I tried submitting several times before the deadline expired with the same result:
"Server Error in '/' Application."

Eventually, I managed to submit a Service Request with the number 1-527191257. This request contains my application for the contest with all the necessary files and comments and the .htm file with the server error. I hope you will accept my contest entry considering there was a server problem and I have put quite an effort for developing my application. Please let me know about my entry status.

Andrei Boeru

0 Kudos
Reply

3,554 Views
RichTestardi
Senior Contributor II
Hi,
 
I attempted to submit a contest entry twice, and both times I got the following error, in red.  Has anyone done a successful submission yet?  Thanks!
 
-- Rich
 
Server Error in '/' Application.
Runtime Error
0 Kudos
Reply

3,554 Views
RichTestardi
Senior Contributor II
Just to follow up and save anyone else the trouble, I received this from Freescale:
 
Our web team indicates that this error occurred because the contest
application servers detected a potentially malicious entry. More
specifically "<Enter>", it is the less than & greater than symbols that
caused the problem.  We are in the process of fixing this, in the mean
time please try entering it as "[Enter]".
 
Sure enough, I had the string "<Enter>" included in the "steps to run" text field, and that was the issue -- I changed it to "[Enter]" and it worked!
 
-- Rich
0 Kudos
Reply

3,554 Views
MCUman
Contributor I
Neither Freescale, Allied, nor Arrow had any boards available as of December 11th. Read Jon Titus' blog about this kit at the dev-monkey.com Web site:
http://www.dev-monkey.com/blogs/jon_titus.php?mid=446
0 Kudos
Reply

3,554 Views
spock_78
Contributor I
Hi,
 
I want to take part in the contest; now I read that the judges will test the entries with a Rev. C board. But I only have a Rev. B board?! Does this mean, I can't take part with my board and that I have to get a new one??
 
 
Thanks for an answer!
0 Kudos
Reply

3,554 Views
JimDon
Senior Contributor III


    And if you try and order one, it says not available for ordering.


0 Kudos
Reply

3,554 Views
JimDon
Senior Contributor III
This have been fixed- however the board will not be shipping until Nov. 26th.
Hope you can code quickly, that will give you about 3 days to complete it.





Message Edited by JimDon on 2008-11-19 12:43 PM
0 Kudos
Reply

3,554 Views
mnorman
NXP Employee
NXP Employee
There was a problem with the Buy Direct system, but that has been cleared up now.  The system may still initially report a long-lead ship date, but if that does occur you will get a follow up message soon after with a revised ship date.  These boards are in stock and ship almost immediately.

The RevB board can be used for developement, and any application written for the RevB board will run on a RevC board.  Note in the board errata document that the only difference is a fixed IR emitter in the RevC version.

The contest deadline is December 31, 2008.   All the details are here: http://www.canyourbadgedothis.com/.  Also check out the YouTube videos with contest rules and JM Badge Board demo and the bottom of that page.

-mnorman


Message Edited by mnorman on 2008-11-21 02:51 PM
0 Kudos
Reply

3,554 Views
JimDon
Senior Contributor III

   Sorry my mistake on the deadline. You actually have 4 weeks, and I did get a notice today that it  has shipped.




0 Kudos
Reply