JM Badge Board Bootloader Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JM Badge Board Bootloader Problem

Jump to solution
2,278 Views
SvmPrasad
Contributor I

Hi,

 

When I connect my JM Badge board to Computer's USB, it runs the message "Press E4 for Bootloader" continuously. After pressing E4 key, left 4 columns of LED light up.

 

After downloading the .S19 file it doesn't work properly.

 

Regards,

SVMP

 

 

 

Message Edited by svmp on 2009-12-09 04:33 AM
Labels (1)
0 Kudos
Reply
1 Solution
1,463 Views
mnorman
NXP Employee
NXP Employee

It sounds like the main application is broken.  The bootloader message "Press E4..." will timeout and attempt to start the application if you do not press E4 soon enough.  It sounds like it is trying to start this application and failing, which resets the hardware and it starts over with bootloader.  Did you follow the steps as outlined in this post to reprogram the original image?

 

Message Edited by mnorman on 2009-12-16 08:41 PM
Message Edited by mnorman on 2009-12-16 08:43 PM

View solution in original post

0 Kudos
Reply
1 Reply
1,464 Views
mnorman
NXP Employee
NXP Employee

It sounds like the main application is broken.  The bootloader message "Press E4..." will timeout and attempt to start the application if you do not press E4 soon enough.  It sounds like it is trying to start this application and failing, which resets the hardware and it starts over with bootloader.  Did you follow the steps as outlined in this post to reprogram the original image?

 

Message Edited by mnorman on 2009-12-16 08:41 PM
Message Edited by mnorman on 2009-12-16 08:43 PM
0 Kudos
Reply